Eaton Logo

Why does the Event Recorder in PowerPort-E continuously show new events?

If the event recorder in PowerPort-E continuously shows new events:

1. Look inside the Event Recorder which protection function is creating the events.
2. Check the settings of this protection function. Adapt them, if necessary. Example: Protection function df/dt (ROCOF) is configured too sensitive and is creating alarms with high frequency. Change the settings of this function.