Eaton Logo

Why can't I synchronize the time on my E-Series Relay?

Please check the following issues:
  • Is the correct protocol for time synchronization selected (<Device Para/ Time / TimeSync>)?
  • Is the timezone set correctly?
  • Open the status page of the used protocol. Check, if the module works correctly.
  • IRIGB: Is the correct type (IRIGB-00x) selected?
  • SNTP: Is the IP address of a valid NTP Server configured?