Eaton Logo

How do I transfer device parameters from one E-Series Relay to another?

To transfer device parameters, both relays must be of the same type (both EDR-5000, for example).

Download the device parameters with PowerPort-E from the first relay. Save them into a file.
 
Now reopen this file with PowerPort-E. Adapt the settings to the order code of the second device <Edit/Modify Device Configuration (Typecode)...>. Select <Apply>. By this the existing parameter file is being converted to the format of the second device.
 
Now there may be incompatible parameters. They are marked with a question mark. These are not valid for this device type. Please adjust the values of these parameters. Afterward you can transfer the parameter settings to the second device.
 
Watch this video for a demo:  https://www.youtube.com/watch?v=k4WDT9QMC_Y