Eaton Logo

Can the PXMP be installed in a separate enclosure?

Yes, the PXMP is available for purchase in an enclosed unit which mounts to the wall. Conduit leads will then be required for the voltage runs and the current sensor runs.  This option is good in retrofit applications. 
 
On new projects, where the majority of the current sensors are installed in the Switchboard/Panelboard, installing the PXMP in the
Switchboard/Panelboard as an integral assembly will be the most desirable.
 
Currently the PXMP is designed to fit in a PRL4 panelboard and Pow-R-Line C switchboards.