Eaton Logo

Can WAGES (Water, Air, Gas, Electricity, and Steam) pulses be input into the PXMP base unit?

The PXMP meter base is equipped with three digital inputs that can be configured as pulse inputs. In addition, an optional Pulse Input Module
(PXMP-PIM) containing eight individual pulse inputs is available.  You can have up to 10 PXMP-PIM modules on a meter base.