Eaton Logo

What is the maximum distance I can have between a PXMP display and the meter base?

Communication of the display is based on Modbus RTU, so distances of 4000 ft are possible. If the display is going to be mounted separately from the power equipment, a 24V DC power supply is required at the display.