Eaton Logo

What is the accuracy of the PXMP system?

The PXMP system, using the 10mA and 100mA meter modules meets ANSI C12.20 0.5% accuracy.
 
Using the 333mV sensors, system accuracy is approximately 1.0%.