Eaton Logo

What types of current sensors metering modules does the PXMP base unit accept?

The PXMP meter base offers 3 types of meter modules:
  • The 100mA meter module is available in125A, 250A and 400A solid core sensor ratings
  • The 10mA meter module supports the CS005 interface to standard 5A current transformers
  • The 333mV meter module can be used with any double insulated 333mV current sensor

These meter modules can be mixed and matched in any of the 10 available PXMP base unit slots.