Eaton Logo

What are the minimum hardware components of a “Standard” PXMP?

Standard hardware consists of the:
  • PXMP Meter Base (10 slots available)
  • PXMP Metering Modules
  • Current Sensors (plug into Metering Modules)
  • Current Sensor cables
  • A 24Vdc power supply

Optional equipment consists of:

  • Web-View Ethernet Energy Portal Module (must be in slot 10)
  • PXMP 6” color touchscreen
  • Pulse input cards (8 inputs)
  • Digital output cards (8 outputs). 

The PXMP requires at least one metering or I/O module to be installed.