Eaton Logo

Can I order an Enclosed Meter without a display?

The PXMP, PXBCM and PXM4000/6000/8000 enclosed meters are available with or without a display.
 
The IQ35M has an integral display.
 
The IQ100/250 and PXM2000 enclosed meters can be ordered as transducer only, which would eliminate the display.  However, if a remote display is required at a later date, we do not have one that works with these meter styles.
 
For more information, visit the Enclosed Meter page.